History#
Version 11 (December 2023)#
- Updated product image in overview topic.
Version 10 (July 2023)#
- Updated the documentation for the Framegrabber SDK release 5.11.0. For a detailed list of all changes, see the Release Notes topic.
- Updated the applet documentation for the CXP-12 Interface Cards and the imaWorx CXP-12 Quad frame grabber. Additionally, the following new applet documentation is now available:
- Line scan applet documentation for the CXP-12 Interface Cards
- FGLib variant of the applet documentation for all CXP-12 Interface Cards
Version 09 (May 2023)#
- Framegrabber SDK:
- Added issue 272272 to the list of known issues.
- Moved issue 197430 from the list of known issues to the list of fixed issues.
- Revised instructions in the "Installing the Driver for Frame Grabbers" section in the Installing the Framegrabber SDK topic.
- Updated bandwidth specifications in the imaWorx CXP-12 Quad Acquisition Applets topic.
Version 08 (February 2023)#
- Added the "Processors" section to the System Requirements for Framegrabber SDK 5.10.0 topic.
- Added further discontinued frame grabbers to the "Discontinuations" list in the Changes and Fixed Issues in Framegrabber SDK 5.10.0 topic.
- Added a known issues entry regarding the PATH environment variable for Windows 32-bit installations. See Known Issues Framegrabber SDK 5.10.0.
- Added the Determining the Frame Number Using the Framegrabber API knowledge article.
Version 07 (December 2022)#
- Revised the entire documentation. Design and wording are now in line with Basler's documentation style. Also, most frame grabber content is now searchable via the search function.
- Restructured the frame grabber documentation to match the structure of the Basler Product Documentation. Separated hardware-specific and software-specific topics.
- Added the imaWorx CXP-12 Quad documentation.
- Renamed the Runtime software to "Framegrabber SDK" and updated the documentation for Framegrabber SDK release 5.10.0. For a detailed list of all changes, see the Release Notes.
- Updated the applet documentation. The applet documentation now appears in Basler's documentation style.
Version 06 (June 2022)#
- Moved the following topics from this documentation to the "Acquisition Cards" section of the Basler Product Documentation:
- Configuring a CXP-12 Interface Card
- CXP-12 Interface Card 1C
- CXP-12 Interface Card 2C
- CXP-12 Interface Card 4C
- CXP-12 Interface Cards
- Updating the Firmware of a CXP-12 Interface Card
Version 05 (May 2022)#
- Linked all mE5 frame grabber documentations to the correct Runtime release notes.
Version 04 (March 2022)#
- Revised the Configuring a CXP-12 Interface Card topic.
Version 03 (October 2021)#
- Moved the following products from the "PC Cards" section of the Basler Product Documentation to this documentation:
- CXP-12 Interface Card 1C
- CXP-12 Interface Card 2C
- CXP-12 Interface Card 4C
- Removed the following discontinued products from the documentation:
- microEnable IV AQ4-GE
- microEnable IV AQ4-GPoE
- microEnable IV VQ4-GE
- microEnable IV VQ4-GPoE
Version 02 (September 2021)#
- Added link to the documentation of the Basler imaWorx CXP-12 Quad frame grabber.
Version 01 (February 2021)#
Content is based on the "Frame Grabbers" section of the Basler Product Documentation (AW001406), version 45, with the following changes:
- Revised the Frame Grabbers topic.
- Added the "Models" section and the Frame Grabber Models topic.
- Updated design and wording in line with Basler's documentation style.