Operator ClipHigh

Operator Library: Arithmetics

The module ClipHigh limits the values to a parametrizable maximum. If the input exceeds the maximum it is clipped, i.e.

I/O Properties

Property Value
Operator Type O
Input Link I, data input
Output Link O, data output

支援的 Link 格式

Link Parameter Input Link I Output Link O
Bit Width [1, 63] 無符號,[2, 63] 有符號 as I
Arithmetic {unsigned, signed} as I
Parallelism any as I
Kernel Columns any as I
Kernel Rows any as I
Img Protocol {VALT_IMAGE2D, VALT_LINE1D, VALT_PIXEL0D} as I
Color Format VAF_GRAY as I
Color Flavor FL_NONE as I
Max. Img Width any as I
Max. Img Height any as I

參數

設定為
Type static/dynamic read/write parameter
Default 127
Range Range of the input link

This parameter defines the maximum value for the output link. If you set the parameter to Static, the value is selected at design time and can't be changed during runtime. If you set the the parameter to Dynamic, you can change the value during runtime.

使用範例

The use of operator ClipHigh is shown in the following examples: