Operator Library: Filter
Operator MAX 會識別並輸出輸入 kernel-stream 的最大值。 此最大值會輸出至 O。 該 operator 不會輸出最大值的 kernel 索引。
| Link Parameter | Input Link I | Output Link O |
|---|---|---|
| Bit Width | [1, 64] 無符號,[2, 64] 有符號 | as I |
| Arithmetic | {unsigned, signed} | as I |
| Parallelism | any | as I |
| Kernel Columns | any | 1 |
| Kernel Rows | any | 1 |
| Img Protocol | {VALT_IMAGE2D, VALT_LINE1D, VALT_PIXEL0D} | as I |
| Color Format | VAF_GRAY | as I |
| Color Flavor | FL_NONE | as I |
| Max. Img Width | any | as I |
| Max. Img Height | any | as I |

上一頁