Operator XOR

Operator Library: Logic

The operator XOR performs a bitwise logical XOR (exclusive OR) operation. Each output bit is set to a logical "1" if the sum of the corresponding input bit values is odd, otherwise the output is "0". The number of input links has to be selected at the instantiation of the module.

Thus the output bit i of n inputs is

I/O Properties

Property Value
Operator Type O
輸入連結 I0, data input
I1..In-1, data input
Output Link O, data output

支援的 Link 格式

Link Parameter 輸入連線 I0 Input Link I1..In-1 Output Link O
Bit Width [1, 64]1 as I as I
Arithmetic {unsigned, signed} as I as I
Parallelism any as I as I
Kernel Columns any as I as I
Kernel Rows any as I as I
Img Protocol {VALT_IMAGE2D, VALT_LINE1D, VALT_PIXEL0D, VALT_SIGNAL} as I as I
Color Format any as I as I
Color Flavor any as I as I
Max. Img Width any as I as I
Max. Img Height any as I as I

1

The range of the input Bit Width is [1, 64] for unsigned values. For signed inputs, the range is [2, 64]. For unsigned color inputs, the range is [3, 63] and for signed color, the range is [6, 63].

參數

無

使用範例

The use of operator XOR is shown in the following examples:

  • "Morphological Edge"

    範例 - 將二值化侵蝕影像與原始影像進行比較。 若兩者相異,則會偵測到邊緣。